2/6/2009 2:53 PM | |
Posts: 11 Rating:
|
HI, AttachmentNew System.pdf (347 Downloads) |
2/6/2009 4:21 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello MRK, I think this can be do. You have already configured connection in S5 side. Just you need to open *.535 file and to see details about connection. (Use COM535 or COM1430). This will help in S7 side. Using this data in NetPro can easy create ISO transport connection with SEND/RECEIVE protocol. Look at Commissioning and Configuring an ISO Transport Connection between the SIMATIC S5 and SIMATIC S7 via Industrial Ethernet *CP535 is older CP1430 Basicly you need: software that can be open configuration file of CP535. You need to put new MAC address of CP443-1 in each CP535; - Step5 + license; - Step7 + SIMATIC NET + licenses; Hardware - CPs + cables for connection; Hope this helps! regards |
2/13/2009 8:06 AM | |
Posts: 11 Rating:
|
Hi, Thanks for the infermatation. |
2/13/2009 3:07 PM | |
Joined: 3/21/2006 Last visit: 3/30/2025 Posts: 10239 Rating:
|
Hello MRK, You are wellcome! regards |
Follow us on