4/2/2021 11:33 AM | |
Posts: 1 Rating:
|
Hello World, I do not manage to understand how to turn the pumps in a way where the one who has the least hour turns in first etc Input 4 level pear 4 backtracking 4 pump fault 1 energy fault output 4 pumps 1 defaut pump 1 energy fault 1 level one pump is active 4 level deactivate on low level time delay I would like the one who has the least hour to start in firt I made a program myself the V3 but I do not know how to create a priority in the order of the pumps how to manage it with which logic gate second V1 program it is made to me, it works in simulation but impossible to transfer in the logo, can you help me to find the syntax errors or to help me to understand how creates a principle of priority.Thank you in advance AttachmentAPI Pompe Blainville V1.1et V3.zip (492 Downloads) |
Last edited by: RomainNormand at: 04/02/2021 11:49:40 |
|
4/2/2021 3:42 PM | |
Joined: 6/19/2019 Last visit: 9/8/2025 Posts: 743 Rating:
|
Hello, Have you looked at LOGO! - Projects forum seach tab? Link HERE and I think you can find any example what you whant becouse there are a lot examples with pumps. Good luck for seaching |
4/2/2021 4:44 PM | |
Joined: 12/18/2014 Last visit: 9/14/2025 Posts: 35960 Rating:
|
Your problem is a typical LOGO! beginner problem. For all blocks that have an output, these outputs must be interconnected. It does not matter whether these outputs are digital or analog outputs. This is not necessary in simulation mode, a program then also works in simulation. If you then want to transfer then the program to LOGO!, then this does not work. The outputs of these blocks must then be connected to: - either to the input of another block. - or a marker (M or AM) - or an output (Q or AQ). In addition to M and Q, X (open connector) can also be used for digital outputs. If the transfer is aborted, an animated, small "i" is displayed in the lower right corner and the information window opens. The cause of the error is displayed there (see attached video).
AttachmentInfo window.zip (488 Downloads) |
Follow us on