(0)| 3/24/2021 11:30 AM | |
|
Joined: 3/4/2020 Last visit: 6/8/2025 Posts: 30 Rating:
|
I'm working on a CNC machine with a SINUMERIK MCU1720 and TIA Portal v16. I achieved a full comissioning of my axis with the SINUMERIK Operate Commissioning tool (v06_14 HF1). But this tool only gives me acces to parameters, diagnostics and settings of the NC, but nothing about Execution of GCODE programs, debug of subprograms, axis position, etc.. So I tried to use VNC Viewer(UltraVNC Viewer) to get acces to the internal Operate of the NC. The problem is I can't find the way to connect the IPC, or another PC/PG with the NC through VNC viewer. The MCU commissioning manual shows the possibility to upgrade the CNC software using VNC Viewer(you can see the captue attached), but I tried it and VNC always fails the connection. I can make ping with the CNC at X127 port, even connect with TIA Portal, but VNC cannot connect. The only solution I found, as an alternative, is to use 3GL-HMI Commissioning Application: 3GL-HMI Commissioning . It looks it's done to use it as a default HMI app like Operate to load, edit and execute programs at the NC. But we use already Operate BaseOnly for our Customized HMI app and the possibility to use VNC would give us an easyer way to manage and debug the execution of programs. |
Last edited by: Boskyman at: 03/24/2021 11:38:00Last edited by: Boskyman at: 03/24/2021 11:39:52Last edited by: Jen_Moderator at: 03/24/2021 13:15:42Optimized link. Living between Spindles, Waterjet heads and Lasers... |
|
| 4/29/2021 8:57 AM | |
|
Posts: 8171 Rating:
|
Hi Boskyman, you can publish the number of the SR. But please, don't publish any personal data or something like that Best regards, |
Follow us on