(2)| 5/22/2021 7:09 AM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36470 Rating:
|
So you want a scaling from -1,00 to 39,00 bar? What is the output of the transmitter? 0-10V? Or 0/4-20 mA? |
| 5/22/2021 12:22 PM | |
|
Posts: 8 Rating:
|
0-10 v sir |
| 5/22/2021 12:57 PM | |
|
Posts: 8 Rating:
|
Yes. -1 to 39 Bar. But 0 bar at room pressure. When transducer is introduced to vaccum it should comes from 0 bar to -1 bar |
| 5/25/2021 8:07 AM | |
|
Posts: 8 Rating:
|
Thank you. I have finished my project. Can you explain about maximum capabilities of log file in logo 8.fs4 |
| 5/25/2021 8:18 AM | |
|
Joined: 12/18/2014 Last visit: 1/17/2026 Posts: 36470 Rating:
|
If you mean the data log, then read the PDF in the attachment.
AttachmentLOGO! 8 manual 0BA8 2016_07 (FS4) pages 273+274.pdf (458 Downloads) |
Follow us on