(0)| 5/26/2021 2:45 PM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi, When using PLCSim, you need to create TCP/IP or ISO connections instead of using named connections (default for PCS7 projects). You need to compile the OS via those connections and afterwards you need to set the S7 protocol channel to PLCSim. The procedure is described in page 744. You have to follow steps 1 to 7. The rest is only used in conjunction with Simatic batch. AttachmentPLCSIM.pdf (237 Downloads) |
|
If I could help you, you can use the RATE button. Thank you. |
|
Follow us on