(1)| 6/10/2021 2:49 AM | |
|
Posts: 22 Rating:
|
Hi! I was doing an project using function block, but at one point it became too complex to use FBD so I would like to use ladder. I'm using an ihm and that's why some inputs are of the network type, in FBD, it's easy to use the network i/o, but in ladder, the network inputs, where I receive data from the ihm, don't have outputs for me carry out the logic. How can i do this? As you can see, theres no output on network analog input, on the digital to! PRINT SCREEN USING FBD PROG: [snip] PRINT SCREEN USING LADDER PROG: [snip] AttachmentScreenshots.zip (291 Downloads) |
Last edited by: Jen_Moderator at: 06/10/2021 11:32:25Removed links and added files as an attachment. |
|
| 6/10/2021 12:36 PM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36482 Rating:
|
For all with a output. |
This contribution was helpful to
|
|
Follow us on