6/14/2021 10:34 AM | |
Joined: 9/30/2016 Last visit: 8/13/2025 Posts: 946 Rating:
|
Please also see the attached screenshots. I have a setpoint that it should only be possible to change when the user is PTAuser. At the moment it is also possible to change the set point when the user is Operatør. As it can be seen in the screenshot both Operatør and PTAuser are available in the User Administration but I do not get the option to pick neither in "Authorizations" dialog on the Output/input. How do I see what the different labels present in the "Authorizations" dialog means? How do I get the authorization on the setpoint Output/input set to PTAuser? AttachmentFA2A.zip (191 Downloads) |
Follow us on