5/19/2021 7:09 AM | |
Joined: 1/31/2020 Last visit: 4/12/2025 Posts: 3 Rating:
|
When the WinСС server is running (WinCC 7.0, SP3), there is a loss of information in clients (irregular, about once every two months), while there is data on the server, everything is fine with the network connection. It looks like WinCC Explorer hangs. I'm new to working with WinCC, in the Diagnos folder in the PMDiagnose file (attached the archive) I found several suspicious messages suitable for the hang time like this: ------ 2021-05-18 15:51:15.259 - ccProjectMgr.exe GetSecurityInfo failed with error 5: Отказано в доступе. 2021-05-18 15:51:15.314 - ccProjectMgr.exe *** Error: CRTApplication::StopWinCCApplication Process (CAReportMergerX.exe) is terminated already 2021-05-18 15:51:16.055 - ccProjectMgr.exe ControlService:No progress made within the wait hint failed for CCProfileServer with error 0: Операция успешно завершена. 2021-05-18 15:51:16.057 - ccProjectMgr.exe *** Error: CRTApplication::StopWinCCApplication Process (HMRT.exe) is terminated already 2021-05-18 15:51:16.411 - ccProjectMgr.exe ControlService:No progress made within the wait hint failed for CCTlgServer with error 0: Операция успешно завершена. ----- There is nothing suitable for the time in the WinСС_Sys files. Maybe someone will tell me on the right path or the problem is in another? Thank you
AttachmentPMDiagnose.zip (237 Downloads) |
5/19/2021 9:20 AM | |
Joined: 10/3/2010 Last visit: 9/9/2025 Posts: 1568 Rating:
|
May I ask if you use Remote Desktop to connect to your server? If so, is the server freezing a while after disconnecting the session? |
B r g d s , |
|
5/21/2021 10:08 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello pylod_j, You should use the SIMATIC Assessment Suite - Data Collector (SAS-DC) https://support.industry.siemens.com/cs/ww/en/view/65976201 Then create a Service Request, and send the data to the
Georg Berghof |
PS: If this post did really help you, you may use the Rate-button |
|
5/21/2021 2:38 PM | |
Joined: 10/3/2010 Last visit: 9/9/2025 Posts: 1568 Rating:
|
I meant freezing of the WinCC-server might happen within a few hours after disconnecting remote access. |
B r g d s , |
|
6/15/2021 12:11 PM | |
Joined: 1/31/2020 Last visit: 4/12/2025 Posts: 3 Rating:
|
No, this is not related to remote access, there is no correlation. As it became clear now, everything starts with the disappearance of trends (both on the client and on the server), the following messages appear in the WinCC_Sys_XX diagnostic file: 255,15.06.2021,12:55:05:259,1012301,4,,061-TANK-SRV,CCWriteArchiveServer,[\BulkPool.cpp,242]failed to insert into TagCompressed with 0x80040E45(266,2021-06-15 08:47:04,2021-06-15 08:55:03 255,15.06.2021,12:55:05:260,1012301,4,,061-TANK-SRV,CCWriteArchiveServer,[\BulkPool.cpp,242]failed to insert into TagCompressed with 0x80040E45(110,2021-06-15 08:47:04,2021-06-15 08:55:03 255,15.06.2021,12:55:07:416,1012301,4,,061-TANK-SRV,CCWriteArchiveServer,[\DataStoreAlarm.cpp,179]failed to insert into MSARCLONG with 0x80004005(#5094,'2021-06-15 08:55:06.977') 255,15.06.2021,12:55:10:343,1012301,4,,061-TANK-SRV,CCWriteArchiveServer,[\BulkPool.cpp,242]failed to insert into TagCompressed with 0x80040E45(77,2021-06-15 08:45:51,2021-06-15 08:55:08 Digging a little forum, I found similar cases and mention of PH ready. Looked at the files CCTlgCommonArchiving 15.06.2021 09:33:10.764 E CCCTlgCA: COM-exception [0x800401f3] while initializing PH ready 15.06.2021 09:33:10.770 E CCCTlgCA: This instance won't have access to the Process Historian I found it there, but the time of the UTC - it means this is not the source of the problem, but the consequence of the reboot (we have UTC+4 time).In general, the reasons are not yet clear. I attach the file WinCC_Sys_XX AttachmentWinCC_Sys_05_txt.txt (259 Downloads) |
Last edited by: pylod_j at: 06/15/2021 12:11:44 |
|
Follow us on