6/28/2021 10:04 AM | |
Joined: 9/30/2016 Last visit: 8/13/2025 Posts: 946 Rating:
|
Please also see the attached screenshots. I have a WinCC 7.5 project that creates an extra directory. The path to the project file is: C:\vdClientArchive\KALEB5_Rewind\Software\KALEB5SRV01\Eb5srv01\wincproj\KALEB5SRV01 but at some point I also get a new directory with the same name as the full project (and the server it is running on): C:\vdClientArchive\KALEB5_Rewind\Software\KALEB5SRV01\Eb5srv01\wincproj\KALEB5SRV01\KALEB5SRV01 Why is this happening and should I do something (what?) about it or just accept it? AttachmentExDir.zip (169 Downloads) |
Follow us on