(0)| 7/1/2021 6:10 PM | |
|
Posts: 1 Rating:
|
Hello mates Upgraded PCS7 from V8.0 to V9.0 SP3 and combined two projects into one. i now have two engineering stations 1 and 2 of which to open project on Eng station 2 you have to access the multiproject in Eng station one via network. The problem i now have is, i am failing to peform a compile of the AS and OS. i will attach the error messages that l get from the Eng station. The other problem with my multiproject is that one of the pictures on the pictures shows a motor on the top left corner of the OS station whereas when you open the same picture from the OS server, it will be positioned well. look at the attchments. Please refer to attachment and those with expertise please assist AttachmentError messages.pdf (157 Downloads) |
Follow us on