7/12/2021 4:00 PM | |
Joined: 5/16/2018 Last visit: 7/24/2025 Posts: 3 Rating:
|
Had anybody been successfull here? I tried to connect to the serial COM port, but did not get any feedback on the console. Not sure, what I am doing wrong. So after that I connected a Monitor with DisplayPort, but there is no output to the monitor. What am I doing wrong? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/13/2021 07:38:00New subject after splitting |
|
7/14/2021 4:15 PM | |
Joined: 6/22/2021 Last visit: 2/3/2023 Posts: 2 Rating:
|
Hello there , To run this device , follow this steps 1 - You need a SD CARD ( without this , it is not possible ) 2 - Once you have a SD CARD you need to install the image file from IOT 2050 3 - the image is avaliable at forum here ( IOT2050_Example_Image_V1.0.2) . 4 - If you are windows user , you can download a tool to prepare the SD card , like rufus (https://rufus.ie/pt_BR/) to format and install the IOT2-5- imagem on SD Card 5 - With the SD and image installed you will see the info at DP port , with no image or no sd card there is no sign at DP port video 6 - Good luck PS.: Serial communication , i have to enable it on setup from Iot2050 and after that i was possible to get the serial communication works at Node Red Jef AttachmentSIMATIC_IOT2050_Setting_up_V1.0.pdf (490 Downloads) |
Follow us on