(0)| 3/1/2009 6:09 PM | |
|
Joined: 3/21/2006 Last visit: 1/22/2026 Posts: 10244 Rating:
|
Hello Look at Position control with MICROMASTER420 frequency converter and asynchronous motors with USS protocol (Tip 65) hope this will help you. regards |
| 3/1/2009 7:55 PM | |
|
Posts: 767 Rating:
|
Thank you umencho. Tomorrow i see de parameters and contrast de information. Thanks and regards. |
| 3/2/2009 9:58 PM | |
|
Posts: 767 Rating:
|
Hello. The output of uss init done is ok. But in error, uss ctrl, I get 1. Someone can get the settingaccurate for MM420 to communicate with s7-200? To configure using the AOP. Pleasesss
2024 0=0 2025 0=125,178,25,2,156 etc 2027 0=14,125,265,32,25,124 etc where is the error? 2012 0=2 YES???? 2013 0=127 yes???? 2014??? 2015???0=???? 700 0=5 1000 0=5 ...... that needs to change? Thanks |
Follow us on