(0)| 7/20/2021 9:44 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hola, Participantes de muchos países intercambian información en el foro de Siemens, y muchos no entenderían el español. Hemos elegido el inglés como idioma común para asegurarnos de que la mayoría pueda entender las preguntas y respuestas. Por favor escríbanos en inglés en su próxima visita. Hello, Participants from many countries exchange information in the Siemens forum, and many would not understand Spanish. We have chosen English as the common language to ensure that most can understand the questions and answers. Please write to us in English on your next visit. It appears that you have a project in Step 7 v5.x (Simatic Manager) that included certain packages that are missing in your installlation - wcf_appx.dll is a file reuired for an imbedded WinCC Flexible RT program, used to setup an HMI stationlinked to the PLC program. https://www.pconlife.com/viewfileinfo/wcf-appx-dll/ - s7wnfcx.dll is linked to ISO on TCP/IP communications on a S7-300, it is possibly related to ISO services not launched, or a missing CP 1612 card in the PC... https://support.industry.siemens.com/cs/ww/en/view/15048962 Are you working with an uploaded Step 7 project, in which case the WinCC Flexible part of the project are missing? If the WinCC Flexible project was embedded in Step 7, you could try removing the embedded project from the Step 7 program... Hope this helps, |
Last edited by: dchartier at: 07/20/2021 21:49:52 |
|
Follow us on