7/23/2021 3:46 PM | |
Joined: 3/19/2018 Last visit: 8/7/2024 Posts: 1 Rating:
|
Hello all forum users and Siemens experts, I have an issue when trying to connect to an OPC UA server with a CPU 1517 as a client. I will describe the issue below:
The Problems (Bugs): I am using the project from Siemens to test communication with a 3rd party OPC UA Server. I am able to access the server using both OPC Scout and TIA. I managed to get over the previous issues (Bad communication error, Bad certificate) but now I'm still unable to connect to the OPC server. The diagnostic status for this error is: 8089_0000, BadConfigurationError. I suppose this issue is on the server side, but unfortunately there is very limited information available. I'm attaching the server configuration XML file for reference. Any suggestions are very welcome. AttachmentSLIKDAUAConfig.txt (532 Downloads) |
Last edited by: Jen_Moderator at: 07/26/2021 09:11:25Optimized link. |
|
Follow us on