(0)| 7/10/2021 3:18 PM | |
|
Posts: 6 Rating:
|
Dear Friends, There is a 5 axis machine with 2 rotary axes (Rotary Table (B) and the one which holds the workpiece with Tailstock (A)) (image attached). Control is Sinumerik 840D pl (powerline) with NCU v6.5 and HMI v6.4. As a result of maintenance and re-assembly, Machine works perfectly with no error but we get to figure out that the final product (Turbine Blade) is not matched with designed one - there is a 0.6 mm difference when measuring depths of cut of both sides of manufactured blade – So, one possibility is that the distance of B axis with respect to the the plane which passes through A axis and tailstock has been changed. I would like to know how to set the new (modified) origin of intersection of rotary axes or distance between rotary axes A and B and Spindle (the 239.5 and 87.1 numbers in the attached image). Unfortunately, the Sinumerik on this machine doesn’t have any mask or HMI page to set Cycle800, Cycle996, or Traori input parameters (TC_CARR) – due to old version of machine or manufacturer choice, there is no Sinumerik Cycles available but only Manufacturer's Cycles- Is there a way to set these data in this machines somewhere, such as, in Machine Data in NCU, PLC, or in probably system variables in Cycles? There was one post regarding this issue for Sinumerik sl, but nothing for Sinumerik pl. any help would be highly appreciated. AttachmentSinumerik PL - Rotary Axes Distances.zip (424 Downloads) |
| 7/14/2021 9:01 PM | |
|
Joined: 4/28/2015 Last visit: 1/16/2026 Posts: 69 Rating:
|
While only newer controls support the use of TCARR for setting TRAORI parameters, all controls support the original method which uses channel data parameters in the 24500 range. The current documentation has a cross reference of TCARR to TRAFO5 parameters. See section 2.7.4 in chapter F2 of the Special Functions manual at https://support.industry.siemens.com/cs/ww/en/view/109763229 HTH, SteveA |
This contribution was helpful to
|
|
| 7/24/2021 3:21 PM | |
|
Posts: 6 Rating:
|
Dear Steve, Firstly I should thank you for the help. That was fantastic and give us some idea to go ahead. It took me 1 week to study all this transformation chapter and then I went to machine to see what I can do. Here is the result: MD24100 $MC_TRAFO_TYPE_1 = 0 MD24500 $MC_TRAFO5_PART_OFFSET_1 [0,1,2] = 0 MD24510 $MC_TRAFO5_ROT_AX_OFFSET_1 [0,1] = 0 MD24550 $MC_ TRAFO5_BASE_TOOL_1 [0,1,2] = 0 MD24560 $MC_TRAFO5_JOINT_OFFSET_1 [0,1,2] = 0 MD20150 $MC_GCODE_RESET_VALUES [24] = 1 (ORIWKS) MD24570 $MC_TRAFO5_AXIS1_1 [0,1,2] = 0 MD24572 $MC_TRAFO5_AXIS2_1 [0,1,2] = 0 (MD24582 $MC_ TRAFO5_TCARR_NO_1) & (MD24682 $MC_ TRAFO5_TCARR_NO_2) are not even available!!!? Note: I need to let you know that we have 6 of these machines, all same configuration, only one got under maintenance of rotary axes and only this one doesn’t produce the part same as design. The rest are working with no problem. The data above are same for all 6 machines. Results made me more confused. As you can see, all parameters are zero!!?? I am really amazed how other 5 machines work without any problem while there is no transformation information set on these machines? and now I much more wonder how machine kinematics have been defined for this machine by machine builder when actually all kinematic chain data is zero !!?? AttachmentNC_Backup+Machine Kinematics.zip (385 Downloads) |
| 7/26/2021 12:37 AM | |
|
Joined: 4/28/2015 Last visit: 1/16/2026 Posts: 69 Rating:
|
Not sure if it is related, but your backup archive shows that the control does not have the option set for TRAORI (or tool mangement, for that matter). Has something happened to cause the loss of option data? Siemens has a software package (Access MyMachine /P2P) that includes a very useful archive comparison tool called DIFF - see https://mall.industry.siemens.com/mall/en/us/Catalog/Product/6FC58607YC450YA0 It is intended for Solution Line controls but works fairly well for Power Line, except for drive data. Or, you can copy out parameters from NC Active data and use a text file comparison program to check for differences. HTH, SteveA |
This contribution was helpful to
|
|
| 7/27/2021 12:35 PM | |
|
Posts: 6 Rating:
|
Dear Steve, I really appreciate your time for explanation. It is really helpful. However, this time I really didn't get what you meant. I even discussed your explanation with two of my colleagues. but none could understand what you meant.The questions are: 1- What do you mean by "compile cycle"? 2- I checked the Series Startup page. Since "compile cycle" is not clear for me, I didn't find anything relevant on this page. Note 1: I checked all machines cycles. Here is the result: Standard Cycles: Empty (Strange but yes empty) User Cycles: It has some cycles but acc. to Machine builder manual, they are measuring cycles. You may see them as attached plus screenshot. Manufacturer Cycles: Empty Note 2: This machine comes with a software. The programmer uses that software to design the part and choose machine model in post-processor. Is it possible that Sinumerik here, doesn't do anything at all but an interpolation among coords it gets from generated software code? Still it doesn't solve the problem where machine kinematic chain is defined but I just thought it may help you to have an idea. About Drive MD, Thanks a million for your very helpful note. Now I found out where such data can be saved. I was actually suspicious about those BOT files but since I couldn't open them, I didn't know what they include but NC Upgrade consists of series of TEA files which exactly they include Drive MDs. Have more questions, but later I will start another post to ask specific question about this matter. Once again thanks to you for putting precious time on this to read and answer me. AttachmentCycles.zip (274 Downloads) |
Last edited by: fixxxer_ki2 at: 07/28/2021 07:11:09Last edited by: fixxxer_ki2 at: 07/28/2021 07:12:22 |
|
Follow us on