7/31/2021 1:26 AM | |
Joined: 5/19/2021 Last visit: 11/11/2024 Posts: 27 Rating:
|
I have a problem that I can't solve on my own A switch button turns on a motor. When the engine turns on, the switch button become red that signify that the operator can turn off the engine whenever he wishes. but ... in the event that the operator forgets to turn off the engine, I would like to include a countdown timer so that the engine turns off on its own after a while the problem I have is that if the motor stops at the end of the time delay, the button stays red and does not turn green again on its own. I can not find a way to send a low output to the variable at the end of the time delay without maintaining a high output before which interferes with the input of the switch button. Thank you very much for your advice. PS . It's a bit the same problem that I had previously with analogic values actualise parameters with LWE and LSC - Entries - Forum - Industry Support - Siemens which had been solved via VM mapping but in this case I do not believe that it is possible. thanks again Attachmentswitch and timer.zip (494 Downloads) |
7/31/2021 4:54 AM | |
Joined: 12/18/2014 Last visit: 9/28/2025 Posts: 36034 Rating:
|
For me is the problem: I don't see what you make in the LWE project. Please upload the LWE project. |
7/31/2021 10:58 AM | |
Joined: 5/19/2021 Last visit: 11/11/2024 Posts: 27 Rating:
|
In attachment the example. I appreciate your help. Attachmentswitch_and_timer.zip (506 Downloads) |
7/31/2021 2:05 PM | |
Joined: 12/18/2014 Last visit: 9/28/2025 Posts: 36034 Rating:
|
Here my suggestion.
Attachmentpush button and timer.zip (698 Downloads) |
7/31/2021 8:06 PM | |
Joined: 12/18/2014 Last visit: 9/28/2025 Posts: 36034 Rating:
|
It sounds good ... I'm happy for you that it works as you wished .... |
Follow us on