(0)| 8/9/2021 5:51 PM | |
|
Posts: 61 Rating:
|
Hello, how can I automatically acknowledge the alarms from ALM module? My D435 is supplied from UPS and when I turn off the ALM module and the main contactor is de-energized a number of alarms appear. So I can not automatically turn on the ALM, but rather I must manually reset all alarms and then turn on the ALM. Is there any way that the acknowledgment of the alarm could be done with a function? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 08/10/2021 09:06:42New subject after splitting |
|
| 8/10/2021 10:36 AM | |
|
Joined: 4/28/2009 Last visit: 6/3/2025 Posts: 347 Rating:
|
Hello, you can use p1210 for automatic fault reset. With regards Martin |
Follow us on