8/10/2021 9:08 AM | |
Joined: 5/16/2014 Last visit: 9/12/2022 Posts: 7298 Rating:
|
Hello LogicSolut, 1. In order to attach clients, the project needs to be Multi-User --> Yes, you need then an additional Server-license.
--> Yes, Otherwise you could only conneect one Client. Assuming this is true, what specific Win Server OS should we purchase? The local company that put together our PCs for the project has currently offered 2 choices: 1. Server 2019 Essentials 25 CAL --> Essentials is not released for using for WinCC, only Standard or Datacenter. 2. Windows Server 2019 OL 16c (plus Dev CAL). --> You can use Windows Server 2019 Standard or Datacenter with WinCC V7.5 and Serviepack 1 or 2. So I have a few of questions: 1. Which would be the best version to use (assuming it is required at all). --> Windows Server 2019 Standard or Datacenter with WinCC V7.5 and Serviepack 2. 2. Will the clients also need a CAL, or is this connection covered in the Siemens software. --> The WinCC-Clients do not need a CAL. 3. Are there any specifics from Siemens on best practice for building the Server OS --> Recommentation for the configuration of the network, see FAQ: https://support.industry.siemens.com/cs/ww/en/view/868014 Best Regards
|
PS: If this post did really help you, you may use the Rate-button |
|
This contribution was helpful to
2 thankful Users |
Follow us on