(0)| 3/4/2009 5:22 PM | |
|
Posts: 26 Rating:
|
Hello, I Have 2 master CPU (one 416 and one 314) and communication beetven with DP/DP coupler. The network is profibus In HW configuration DP/DPcoupler Release 2 is configured according as picture(see attachment). Is it possible send real values (total amount from flow meters,pressure,etc) from one cpu to the other,if is in object properties in slot of coupler specified unit BYTE,and consistency lenght UNIT see picture. I want used MOVE function and DW format. Thanks AttachmentConsistency.pdf (607 Downloads) |
| 3/5/2009 2:35 PM | |
|
Posts: 26 Rating:
|
Hi Phantom75, Any configuration for DP/DP coupler,and program for transfered data with MOVE function thru DP/DP coupler. |
| 3/6/2009 12:14 AM | |
|
Posts: 2661 Rating:
|
Hi misab, Also look at the following FAQ: What are the special features of input/output addressing with the DP/DP coupler? |
| 3/6/2009 12:35 AM | |
|
Posts: 26 Rating:
|
Thanks Phantom75 Best regards! |
Follow us on