(0)| 3/6/2009 8:15 AM | |
|
Posts: 29 Rating:
|
Hello, take a look at this link: http://support.automation.siemens.com/WW/view/en/14390055 Perhaps it helps you. Regards |
| 3/6/2009 8:36 AM | |
|
Posts: 64 Rating:
|
Thanks, I´ve seenthis faq, but in this information can´t see any information about different power motors. Really thanks Stöppacher. I continue with my search... |
| 3/8/2009 4:18 PM | |
|
Joined: 5/28/2008 Last visit: 1/14/2026 Posts: 4522 Rating:
|
Hello Vagabund, We are talking here to run more than one motor from the same drive. The motors are different. Suppose you have two motors now. You will make the quick commissioning e two times. One will be saved intoDDS[0] "Drive data Set 0" and the other will be saved in DDS[1] "Drive data Set 1". You have to assign a DI to the drive to select between DDS. There is also something calledcommand data source "CDS" You can define more than one and control the motors using many command sources like profibus, terminal , ..etc. Search by "Data Sets"the following manuals: http://support.automation.siemens.com/WW/view/en/24291961 http://support.automation.siemens.com/WW/view/en/24294529 With best regards |
|
Ayman Elotaify |
|
Follow us on