(0)| 9/2/2021 10:03 PM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hi, Take a look at the Industry Library (Link), it features two additional valves: VlvDsL and VlvDiv (see attachment). The VlvDsL is a double seated valve and is drawn as a four way valve. However, the block only features open and close and open/close top and bottom seat. Another option is the VlvDiv which is a diverter valve that can be set to 8 positions max. Maybe one of these block is useful to you? |
|
If I could help you, you can use the RATE button. Thank you. |
|
| 9/3/2021 3:24 PM | |
|
Posts: 2 Rating:
|
Thank you for the feedback. Do you have any information on implementing a three way valve that needs four position (one being closed)? |
Follow us on