(0)| 10/17/2021 5:25 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello lesther roque; The picture you show is done with a cellphone camera, it would be a sharper image if you had generated a screenshot. As far as I can tell, 2 of your online status icons at the bottom of the image show a configuration mismatch and 2 more show a faulty module icon. This is explained in the Programming with Step 7 manual (for Step 7 v5.6), Ch. 23, Diagnostics. Take the time to study this chapter, it will save you headaches in the long run. https://support.industry.siemens.com/cs/ww/en/view/109751825 When any icons of this sort appear in the HWConfig Online View, double-clicking n the icon will open the diagnostic buffer of the module, which should guide you to find the cause of the problem of that module. More information should be available in the CPU's diagnostic buffer,, which is generally more complete. You can use the SAVE AS.. button in any Diagnostic buffer screen to create a text file containing the messages logged in a diagnostic buffer. Attach it here so we can have a look at it, if you need a bit more help. Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 10/17/2021 17:26:11 |
|
Follow us on