(0)| 10/19/2021 2:43 PM | |
|
Joined: 6/4/2020 Last visit: 1/13/2026 Posts: 2 Rating:
|
Hi Vicky Bhau. I don't think you need a managed switch on the above network (see attached screenshot). You need to use the System IP function, per the manual, to speak with HMI devices, using the X2 ports (preferable). Also, have a look at the "HMI Communication" section of the manual: S71500 - Communication I'm starting to play also with a S7-1515R-2 PN with WinCC 7.5 SP1 / SP2. Thanks! |
Last edited by: The Helping Hand at: 10/20/2021 08:42:03Optimized link. |
|
Follow us on