(0)| 11/12/2021 9:43 AM | |
|
Joined: 12/18/2014 Last visit: 1/16/2026 Posts: 36460 Rating:
|
Which LOGO!s have you exactly? Which firmware versions have the LOGO!s? |
| 11/12/2021 9:58 AM | |
|
Joined: 6/19/2019 Last visit: 1/16/2026 Posts: 744 Rating:
|
Hello, First solution do life bit to see or connection drop link HERE Second solution if you whant you can put in first logo TOF function for 1 second to control your pumps so if connection loose for less then 1 second you wont stop your pumps if connection lost more then 1 sec, then it stops and the problem will be solved. |
Last edited by: Jen_Moderator at: 11/12/2021 12:03:18Optimized link. |
|
| 11/13/2021 9:11 PM | |
|
Joined: 12/18/2014 Last visit: 1/16/2026 Posts: 36460 Rating:
|
I think there is a problem with the LAN connection. Working e.g. VFD's in the near? |
| 11/13/2021 9:16 PM | |
|
Posts: 4 Rating:
|
Ill try to do the test when ill be near logo's. I thought about using time delay block , but it's just temporary solution. Becuase i just need to know why this is happening for future understanding. And i also doubled checked last time, it's not that i am losing my inputs. It's just once in 1 hours , SECOND LOGO dsn't send input status to FIRST LOGO or FIRST LOGO dsn't want to receive them sometimes. I can send my project to someone , maybe I don't understand something... |
Follow us on