(0)| 11/25/2021 1:24 PM | |
|
Joined: 2/17/2020 Last visit: 1/15/2026 Posts: 1251 Rating:
|
Hi banconi, This message contains the information that the backups of the WinCC archives cannot be done, until the OS server isn't correct synchronized. Therefore will be postponed the backup until the redundant partner is restarted, the redundant status of the OS (no faulty) is clear and the OS was synchronized. In most cases, the message should disappear after the reboot and finishing of the redundancy synchronization. If not, a further analysis of the installation may be required via a Support Request to Siemens. |
|
A rating will be well appreciated. |
|
Follow us on