12/15/2021 4:24 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35955 Rating:
|
In attachment a simple example.
AttachmentVariabel_setpoint_with automatic_loop_0BA8.Standard.zip (605 Downloads) |
This contribution was helpful to
1 thankful Users |
12/15/2021 7:04 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35955 Rating:
|
Slowly is relative ... There's block with a ramp function. And more then 4 setpoints are possible. See this topic: Time varing analogue output profile |
This contribution was helpful to
1 thankful Users |
12/15/2021 7:40 PM | |
Joined: 12/15/2021 Last visit: 1/3/2022 Posts: 9 Rating:
|
Thank you! I am all in to it know. Great support! all best t |
12/15/2021 7:46 PM | |
Joined: 12/18/2014 Last visit: 9/13/2025 Posts: 35955 Rating:
|
Here's a simple example for the ramp function. You can change the speed in the parameter "Change of speed". - Value higher > changig speed faster. Note: The speed in the simulation is not the same as in a real LOGO!. AttachmentSimple_example_ramp_function_0BA8.Standard.zip (624 Downloads) |
Follow us on