(0)| 10/23/2018 7:57 PM | |
|
Posts: 2 Rating:
|
Hello, I am installing WinCC 7.4 SP1 and I get an error during the SQL installation that then forces the WinCC installation to be aborted and Windows to restart. After if I run the installation again, the error does not appear and WinCC is installed, but then I cannot connect to the SQL server. I have tried all the methods described on the fórum for this issue (Cannot conect to server) and nothing seems to work. I then unistalled WinCC and SQL, and performed a new installation, the same behaviour happened again, installation aborted after an error during the SQL installation. After this the installation runs until the end but then I cannot connect to the SQL server. Attached you can find the log file of the SQL installation just after the error during the installation, can you help please? ------------------------------------------------------------------------------------------ AttachmentSqlSetup.txt (245 Downloads) |
Last edited by: AutoGen_280204 at: 10/23/2018 7:58:19 PMLast edited by: AutoGen_280204 at: 10/23/2018 7:58:47 PMLast edited by: Jen_Moderator at: 10/24/2018 10:00:03 AMNew subject after splitting |
|
| 12/17/2021 3:17 PM | |
|
Posts: 24 Rating:
|
I have the same error code and couldnt make it for more than 1 day. What kind of other ways do you know also? |
Follow us on