(0)| 12/16/2021 9:16 AM | |
|
Joined: 4/28/2015 Last visit: 12/4/2025 Posts: 14 Rating:
|
Hi guys, So WinCC 7.4 without SP1 is vulnerable to this new security bug. I am wondering of what part of WinCC is this referring to. I figured out that it may have be WinCC OPC UA server. If I dont want or dont know how to change log4j2.formatMsgNoLookups parameters, Can I somehow fully disable this feature in WinCC 7.4 if I dont use WinCC OPCUA server? Info: https://cert-portal.siemens.com/productcert/pdf/ssa-661247.pdf SSA-661247: Apache Log4j Vulnerabilities (Log4Shell, CVE-2021-44228, CVE-2021-45046) - Impact to Siemens Products SIMATIC WinCC V7.4: All versions < V7.4 SP1 Update to V7.4 SP1 or later version
WORKAROUNDS AND MITIGATIONS Siemens has identified the following specific workarounds and mitigations that customers can apply to reduce the risk: • If the specific Siemens product allows it: Set the parameter log4j2.formatMsgNoLookups to ‘true’. This measure reduces (but not completely eliminates) the risk for remote command execution via CVE-2021-44228. It does not mitigate CVE-2021-45046. • If the specific Siemens product allows it: Remove the JndiLookup class from the classpath: ’zip -q -d log4j-core-*.jar org/apache/logging/log4j/core/lookup/JndiLookup.class’. This measure mitigates both CVE-2021-44228 and CVE-2021-45046. • If the specific Siemens product allows it: Modify all PatternLayout patterns to specify the message converter as ‘%m{nolookups}’ instead of just ‘%m’. This measure reduces (but not completely eliminates) the risk for remote command execution via CVE-2021-44228. It does not mitigate CVE-2021-45046. • If the specific Siemens product allows it: Update the Log4j component to 2.16.0 or later versions on the systems where the product is installed. This measure mitigates both CVE-2021-44228 and CVE-2021-45046. |
| 12/16/2021 10:36 AM | |
|
Joined: 4/28/2015 Last visit: 12/4/2025 Posts: 14 Rating:
|
In the latest update WinCC 7.4 is removed from the list: https://cert-portal.siemens.com/productcert/pdf/ssa-661247.pdf
|
This contribution was helpful to
|
|
Follow us on