3/20/2009 2:39 PM | |
Joined: 9/27/2007 Last visit: 12/18/2020 Posts: 993 Rating:
|
Hi Rawat To compile the OS double click at "Simatic PC Station" > "WinCC Application" rightclick at the OS-name and select "compile" follow the wizzard. By the way, iallways use this wizzard to comile the OS. to load a single block doubleclick at the block. click in the opened editor at "PLC" > "Download" regards cumulus |
Learn more about visualization - visit the HMI courses of Siemens AG! |
|
3/20/2009 3:40 PM | |
Joined: 4/5/2006 Last visit: 7/30/2025 Posts: 917 Rating:
|
Hi RAWAT, after plc program modification need compile program and download it. System will download everything changed (check box "include user data block", depending from which version you are using). Different possibilities about OS compile, depending from which version are you using: after plc program compilation will be you able to compile OS, as well as cumulussaid, if you are using PCS7 v7 and ES/OS station. for previuos version you have to exit from WinCC runtime to compile OS. if ES is not OS station you need download compiled OS on OS station Hope can help you Regards |
Follow us on