12/12/2021 2:50 PM | |
Joined: 10/8/2019 Last visit: 5/23/2025 Posts: 4 Rating:
|
Hi! Siemens is a big slow self confident multinational company with a large range of products and customers. (My post back then.) Another silly thing was the tag concept in Step 7 classic. I remember my feelings back then I realized tags were just displayable names for memory addresses without any other meaning and function. Tags were no variables. Constants in TIA SCL is a joke. Enums are not supported. Constants are local. It is not possible to use block local constants outside of the block just as constant tags. Why not able the compiler handle this problem at compile time? TIA is Totaly INTEGRATED Portal? Then why I am not able to use constants defined in PLC block on HMI. It is also a compile time problem. SCL portability in between Siemens and Codesys is one way only with additional handwork. ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 12/13/2021 06:50:06New subject after splitting 0x0D0A in big endian |
|
This contribution was helpful to
4 thankful Users |
Follow us on