(0)| 1/5/2022 7:09 PM | |
|
Joined: 9/27/2006 Last visit: 1/16/2026 Posts: 12481 Rating:
|
Hello Sebastian; Without any more specific information (such as the number of connected IO Devices on Profinet, the make and model of the IO lLink masters on Profinet...) al i can tell you is this: -all s7-1500 CPUs come with (at least one) Profinet interface, so they will easily connect to a number of IO devices on your network. The S7-1511C-1PN Cpu, the smallest yu can use, can handle up to 32 IO devices over Profinet (or Profibus with a Profibus CM), see the screenshot below, form the S7-1511C-1PN technical data. - connecting to an SQL database with your S7-1500 CPU is not diffiult, uing T-functions over Profinet, as shpwn in the following Application Example: - Connecting a S7-1200 / S7-1500 to a SQL Database https://support.industry.siemens.com/cs/ww/en/view/109779336 Hope this helps, Daniel Chartier |
Last edited by: dchartier at: 01/05/2022 20:35:11 |
|
| 1/5/2022 7:28 PM | |
|
Joined: 7/29/2013 Last visit: 11/1/2025 Posts: 53 Rating:
|
Hi Daniel, I cant tell you right now the numbers of IO Link masters or Profinet IO modules. But if this help, i will be no more than 25 modules. And until now we use IFM AL1102 IO Link masters.
|
Follow us on