1/8/2022 8:46 AM | |
Joined: 3/30/2020 Last visit: 9/25/2025 Posts: 5477 Rating:
|
@Balex7974: Hello. Your suggestion will work but it is a naïve approach that causes issues when the data points become more. You severely limit yourself for not using SCL. You already have access to arrays, so a for-loop can be used to process the data. I was about to criticize Mr. Einstein for his answer. But then I followed his advise and saw his answer is actually helpful. The library you are looking for is: The function within this library that can be helpful is: LGF_SearchMinMax Regrettably you will have to learn from the code and make your own or convert the TIME values to DINT values. Regards. |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
This contribution was helpful to
1 thankful Users |
Follow us on