(0)| 7/4/2019 3:32 PM | |
|
Posts: 32 Rating:
|
Hello guys! I need help to do a backup (using prosave v15) on a tp 170A. First: i'm using windows 7 professional second: i have with me two cable, and i don't know wich one to use: USB PPI MULTIMASTER CABLE ( 6ES7 901-3DB30-0XA0) SIMATIC S7 ADAPTER USB (6ES7 972-0CB20-0XA0 In first image i can't select the com port because dont appear in my pc. if i select mpi profibus, i have to add an op address according hmi.. but anyway fail.. I checked on hmi and i see dip switch but idk if i need to change it... ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 07/05/2019 08:22:11New subject after splitting |
|
| 2/9/2022 7:56 PM | |
|
Posts: 1 Rating:
|
Did you figure this out? I am currently working on the same issue with a TP170A |
Follow us on