(0)| 2/10/2022 10:21 AM | |
|
Joined: 10/26/2011 Last visit: 1/13/2026 Posts: 766 Rating:
|
Hello, If you are using PCS 7 V9.1, we recommend to use Industry Library (IL) V9.1. If you want to use IL V9.0 with PCS 7 V9.1, you have to consider a few things. In this case you have to use APL V9.0 SP3 and Basis Library V9.0 SP3, see note in Compatibility Tool. You have to install the APL and Basis Library after installing the IL. Compatibility Tool SIMATIC PCS 7 Libraries |
Last edited by: Thunderstorm at: 02/10/2022 10:23:44SIMATIC PCS 7 - Overview |
|
| 2/11/2022 10:49 AM | |
|
Joined: 10/26/2011 Last visit: 1/13/2026 Posts: 766 Rating:
|
Hello Techno Taru, your screenshots shows what I have described. No SP1 to IL V9.1 exists yet. IL V9.1 without SP1 is released with PCS 7 V9.1 as well as PCS 7 V9.1 SP1. For an update to PCS 7 V9.1 (SP1) without utilization of new functions you have to use the APL V9.0 SP3 Upd6 and Basis Lib V9.0 SP3 Upd6. Unfortunately there is no release for IL V9.0 SP3 for PCS 7 V9.1 SP1 only for PCS 7 V9.1 without SP1. Therefore you can update to PCS 7 V9.1 without SP1 only. |
|
SIMATIC PCS 7 - Overview |
|
Follow us on