(2)| 2/8/2022 4:44 PM | |
|
Joined: 2/4/2021 Last visit: 12/8/2025 Posts: 16 Rating:
|
If anyone can help a bit further I'm not able to add a newline to the Wstring. I believe new line is hex 0D I've tried a few combinations that wouldnt go into the Deafult value box, such as 0D $0D , but if I try '$0D' it immediately changes to WSTRING#'$R' so I think I'm onto a winner. When I run the HMI simulation my textbox says "Test_bool_1""Test_bool_2" great to see it has the two tagnames as expected, but unfortunately no new line between them. In the PLC the monitored value of the Wstring is WSTRING#'"Test_bool_1"$R"Test_bool_2"$R' so the $R is in there but HMI not displaying it. Any ideas? ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 02/09/2022 05:56:49New subject after splitting |
|
Follow us on