(0)| 2/16/2022 7:59 AM | |
|
Joined: 4/22/2018 Last visit: 9/23/2025 Posts: 57 Rating:
|
Does nobody have any idea? |
| 2/17/2022 8:18 AM | |
|
Joined: 5/3/2017 Last visit: 12/5/2025 Posts: 673 Rating:
|
Hi Ali_Nickandish95, If you already use blocks in the user program that have the same block numbers, there is a block number conflict. So you have to rename this blocks. But you have to consider that you can only rename the blocks that are called directly in the user program, but not the blocks that called in the block itself. So you have two options to rename the block:
With regards |
Follow us on