(0)| 2/18/2022 3:51 AM | |
|
Posts: 3 Rating:
|
Hi all, I'm having an issue in online a Siemens TP1200 comfort panel (IPC) using a translated IP by 1783-NATR. I do not have issue in connecting the PLC through translated IP, but I cannot online the HMI even after enabled the ports for the translated IP by referring to https://support.industry.siemens.com/cs/document/80917729/which-ports-are-used-by-wincc-advanced-wincc-runtime-advanced-wincc-runtime-professional-basic-panels-comfort-panels-panels-and-ipc-?dti=0&lc=en-WW Do refer the attachment for the network connection. Thus, may I know do I enabled the wrong ports or I miss out some setting to be done in IPC? Thanks. |
| 2/22/2022 2:43 PM | |
|
Joined: 8/3/2009 Last visit: 1/19/2026 Posts: 16644 Rating:
|
Hello Shu Fangg If you want to get access from outside of a subnet (for example with VPN or similar) you should also consider this FAQ: https://support.industry.siemens.com/cs/ww/en/view/109781206 Perhaps it helps. Bye Murof |
|
If this Information really helps, you could use the Rate function |
|
Follow us on