(0)| 3/1/2022 6:05 PM | |
|
Posts: 257 Rating:
|
As a successor to the SIMATIC Panel TP177B, we recommend the SIMATIC Panel TP700 Comfort. Why are there two variants of the SIMATIC Comfort Panel TP700? The reason is that the specified order variant: 6AV2124-0GC01-0AX0 (SIMATIC HMI TP700 Comfort) is a panel for use under standard conditions (media air load, temperature range, installation heights, etc.). The second variant: 6AG1124-0GC01-4AX0 (SIPLUS HMI TP700 Comfort) is a SIPLUS device developed for extended environmental conditions. SIPLUS HMI systems are optimised for visualisation under extreme environmental conditions. The SIPLUS Comfort panels are characterised by the following extended properties, among others:
Important notes on migration from TP177B to TP700 Comfort The SIMATIC HMI Operator Panel Migration Guide contains important information on the topics: Project planning aids, comparisons regarding display dimensions and resolution, housing dimensions, installation cut-outs, etc.. Further sources of information Migration of SIMATIC panels/PC stations to WinCC (TIA Portal) Migration of plants with SIMATIC (TIA Portal) - Visualisation Best regards, SIMATIC International Technical Support Hub |
Follow us on