(0)| 1/15/2022 7:24 AM | |
|
Posts: 4 Rating:
|
Hello dear friends, I hope you are well. I have the following problem: I have configured my iot2050 advanced and I can not access from my laptop to it using ssh connection (putty) through the ethernet cable connected to the LAN P2 port. I have been able to configure the equipment using UART communication by placing the following data on the network interfaces: eth0 : 192.168.1.13 eth1: dhcp laptop: 192.168.1.9 Although I can't connect via ssh, I can ping from my laptop to the iot and I can also access the network node as shown in the images. When I try to access via ssh in the serial terminal I get the message "no supported key exchange algorithms [preauth]". I would greatly appreciate your help.
Attachmenterror ssh connection.pdf (631 Downloads) |
Follow us on