(1)| 3/3/2022 8:35 AM | |
|
Posts: 4 Rating:
|
Yes, thkink that I configured it all properly. Take a look at attachments: |
| 3/3/2022 8:36 AM | |
|
Posts: 4 Rating:
|
|
| 3/3/2022 8:36 AM | |
|
Posts: 4 Rating:
|
|
| 3/3/2022 9:05 AM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36482 Rating:
|
At first glance this looks correct. But I would change the address of the LOGO! change, I would not leave the device address at 1, but use 3 or another. Unfortunately I can't test because I don't have a real KP300. I have only found in tests with simulated HMIs that communication with a LOGO! 8.0, LOGO! 8.1 and LOGO! 8.2 is possible, but not with a LOGO! 8.3. I cannot say whether the new security features of the LOGO! 8.3 prevent communication with an HMI. If I were you, I would ask Siemens, please start a Support Request. |
| 3/3/2022 9:29 AM | |
|
Joined: 4/24/2006 Last visit: 1/16/2026 Posts: 9105 Rating:
|
Hi, What version of TIA Portal do you use? Best regards, Wizard |
| 3/3/2022 9:55 AM | |
|
Posts: 399 Rating:
|
There are FAQs which descripts your application, e.g. a simple one: https://support.industry.siemens.com/cs/ww/en/view/56348902 The FAQ uses old versions, but you can use it with the actual once too. You describe how you define IP parameters, enable S7 communication and the connection in HMI. But it seems you forget to create a server S7 connection in LOGO!, see the FAQ. |
Last edited by: LOGO! Support at: 03/03/2022 09:57:32 |
|
| 3/3/2022 10:35 AM | |
|
Joined: 12/18/2014 Last visit: 1/19/2026 Posts: 36482 Rating:
|
Here a screen video from a test between a simulated SIMATIC HMI and a LOGO! 8.2. There are long pauses between the display on the HMI, because at the beginning and in between I switched off the power supply of the LOGO! and the switch so that you can see that the connection from the HMI to the LOGO! is not set up, but only when the LOGO! and the switch is powered. The length of the pauses is due to the fact that my switch takes 30 seconds to start working. AttachmentTest simulated HMI with real LOGO! 8.2.zip (340 Downloads) |
Follow us on