(0)| 3/4/2022 8:03 PM | |
|
Posts: 257 Rating:
|
In principle, all devices of the SIMATIC Comfort Panels family are available for this purpose. However, a combination of SIMATIC Panel IPC and WinCC Runtime Advanced or WinCC Runtime Professional would also be possible. The runtime option "WinCC Audit" provides additional functions for Comfort Panels or WinCC Runtime Advanced in order to achieve a GMP-compliant application. (see also manual, especially chapter 5.1.9 and chapter 7). The manual also describes strategies for creating GMP-compliant applications with WinCC Runtime Professional. The user administration of the HMI is linked to the Active Directory via the SIMATIC Logon and (optionally) PM-LOGON options. Best regards, SIMATIC International Technical Support Hub |
Last edited by: Jen_Moderator at: 03/07/2022 10:46:40Edited text for better reading. |
|
Follow us on