(0)| 3/31/2009 2:05 PM | |
|
Joined: 5/28/2008 Last visit: 9/1/2025 Posts: 901 Rating:
|
and the function from SP1 is the same like the control in your panel |
| 3/31/2009 2:31 PM | |
|
Posts: 17 Rating:
|
Thank you very much... If i understand this correctly, then I need to implement this function SetDaylightSaving and somehow calculate when this daylight change is happening and the activet/deactivate this function to get the panel to change automatically. If that is the solution, then I believe that this is a poor solution, for something that common as daylightsaving change.... //Brian |
| 3/31/2009 4:36 PM | |
|
Joined: 4/24/2006 Last visit: 1/20/2026 Posts: 9106 Rating:
|
Dear tisbris, Perhaps the following links might be helpful: http://support.automation.siemens.com/WW/view/en/19324378 http://support.automation.siemens.com/WW/view/en/26961516 Best regards, Wizard |
Follow us on