(0)| 1/8/2022 8:13 AM | |
|
Posts: 3 Rating:
|
Hello Ok, thank you for your answer. The frequency is max 40 Hz, so its low speed. Can i do somewith with a timer? |
| 1/8/2022 8:19 AM | |
|
Joined: 12/18/2014 Last visit: 1/22/2026 Posts: 36503 Rating:
|
40 Hz, then must it be possible. Overlap the signals? Are you a encoder? Give more details. |
| 1/19/2022 4:41 PM | |
|
Posts: 1 Rating:
|
Hi I send this small program in logo, For higt frecuencies not more than 5 khz supose have to work. Inputs I4 and I5 in a Logo24CE (Fast inputs) And in tge outputs have the sense wich signal came first, I used in small encoders where have 2 signals A and B and low frecuencies but if you are looking for logo for something like this can works. ADPC328
AttachmentDet Cuad A-B.zip (475 Downloads) |
| 3/11/2022 7:06 AM | |
|
Posts: 8171 Rating:
|
New question published by JOHNAK is split to a separate thread with the subject Would like to activate one output for clockwise rotation and another for counterclockwise rotation. Best regards |
This contribution was helpful to
|
|
Follow us on