(0)| 4/11/2022 4:55 PM | |
|
Joined: 6/3/2013 Last visit: 11/17/2025 Posts: 50 Rating:
|
Hi, Test with the Setpoint greater than the PV and check if the output goes down. Check Reverse Operation option. See: TIP: PID (FB PID_Compact) V2.x (configured with STEP7 V12) |
|
And you will know the truth, and the truth will set you free. |
|
| 4/12/2022 1:31 PM | |
|
Posts: 23 Rating:
|
If the SP is greater than the Input/PV then the Output still ramps up |
| 4/12/2022 1:45 PM | |
|
Posts: 5521 Rating:
|
hi Neogazz_Alpha, can you show us a screenshot of the online view of the block? regards, |
| 4/12/2022 2:55 PM | |
|
Posts: 23 Rating:
|
See attached picture. As you can see the output just ramps up to 100% even though the SP is lower than the Input/PV. Any ideas why? |
Follow us on