(0)| 4/7/2009 8:57 AM | |
|
Joined: 4/5/2006 Last visit: 10/3/2025 Posts: 917 Rating:
|
Hi Victor, you & Rosalieare both right: Siemens says no more than 4 clients on same server, reason is performance. Siemens usually tests HW & SW (Rack PC & PCS7 application) in standard configuration; PCS7 project database average size, compatibilities with addon tools like WebNavigator and so on..... At the end Siemens suggest a typical configuration for good performance in each situation, but you can use different architecture (with more than 4 clients if your PCS7 database is smaller or PC from different customer) in according with your application. The trouble could raise from tecnichal support: they usually follow very strong the raccomandation. In conclusion, if you are using standard application and it's working good for you. If you are planning to use addon like WebNavigator or other application i suggest you to ask your salesman before do it, to avoid fastidius problem could occours when plant will be running (some special application need Microsoft license also) Regards |
| 4/7/2009 2:01 PM | |
|
Posts: 20 Rating:
|
Hi CBo and Rosalie, |
Follow us on