(1)| 4/20/2022 5:46 PM | |
|
Joined: 2/17/2020 Last visit: 1/19/2026 Posts: 1251 Rating:
|
Hi -dFx-, I understand that server and client have exactly the same version of WinCC installed, including SP and Updates, right? The version of STEP 7 V5.5. SP3 is not compatible with WinCC V7.0 SP2, so it might be advisable to install ServicePack 3 of WinCC V7.0, which does support this compatibility. It is important that the terminal bus (Server-client) is separated from the plant bus, each bus with its own network card, to avoid connection problems. I would also check the compatibility between WinCC and the operating system of the server PC and client PC, using the tool below: Welcome to the compatibility tool Finally, the points indicated in this FAQ must be met: What are the requirements for operating SIMATIC WinCC in a Windows network? |
|
A rating will be well appreciated. |
|
This contribution was helpful to
|
|
Follow us on