(0)| 4/30/2022 5:12 AM | |
|
Joined: 3/14/2013 Last visit: 11/29/2023 Posts: 1 Rating:
|
i want to install IOT2050_Example_Image_V1.2.2.zip (780,6 MB)(SHA-256) Win32DiskImager,and reboot it has same error who can tell me?why? error is: switch to partitions #0, OK mmc0 is current device switch to partitions #0, OK mmc1(part 0) is current device ====== uuid conflict check end ====== switch to partitions #0, OK mmc0 is current device Scanning mmc 0:1... Found U-Boot script /boot/boot.scr 704 bytes read in 1 ms (687.5 KiB/s) ## Executing script at 83000000 Loading /usr/lib/linux-image-5.10.64/... ** File not found /usr/lib/linux-image-5.10.64/ ** Loading /boot/vmlinux-5.10.64... 18296840 bytes read in 4572 ms (3.8 MiB/s) ERROR: Did not find a cmdline Flattened Device Tree Could not find a valid device tree SCRIPT FAILED: continuing... |
| 5/3/2022 9:18 AM | |
|
Joined: 4/28/2015 Last visit: 1/15/2026 Posts: 3345 Rating:
|
Hi, for using the Example Image V1.2.2 you at first need to update the firmware of the IOT2050. For more details see here. Best regards! |
|
Not working for IOT2050 support anymore from March 1st, 2024. |
|
Follow us on