5/5/2022 5:01 PM | |
Joined: 2/21/2022 Last visit: 6/7/2023 Posts: 15 Rating:
|
Looking for a way to add a message text in LOGO 1 with a timer preset where the timer block is in the LSC file in LOGO 2. |
5/5/2022 5:47 PM | |
Joined: 12/18/2014 Last visit: 9/25/2025 Posts: 36032 Rating:
|
Her's a example. Take a look at Parameter-VM-Mapping. In LOGO!s must the timer have the same time base. AttachmentSet_timer_value_remote_FS4.zip (552 Downloads) |
5/6/2022 12:28 PM | |
Joined: 2/21/2022 Last visit: 6/7/2023 Posts: 15 Rating:
|
Does it work in simulation or do I have to have two LOGOs on a physical network? |
5/6/2022 12:31 PM | |
Joined: 12/18/2014 Last visit: 9/25/2025 Posts: 36032 Rating:
|
The simulation mode of LSC simulate not all. I have tested the solution with 2 LOGO!s FS4. |
Follow us on