(1)| 5/24/2016 7:34 AM | |
|
Joined: 3/14/2008 Last visit: 1/19/2026 Posts: 2233 Rating:
|
Hello, Did you do the following? 1. Open the SIMATIC Manager and activate the plant view. 2. Select the required hierarchy folder in the tree view. – If you want to create diagnostics screens for the multiproject/project, select the multiproject/project. – If you wish to create diagnostic screens for certain hierarchy folders, select the required hierarchy folder in the maintenance station. 3. Select the Options > Plant Hierarchy > Create/Update Diagnostics Screens menu command. 4. If you have already compiled the AS charts, no other dialog box is opened, and the diagnostic screens are created/updated directly. Proceed to step 6. 5. If you haven't compiled the AS charts yet, the "Create module drivers" dialog box is opened one after another for every CPU for which this function has not been executed yet. Click "OK" in all dialog boxes to create the required diagnostic blocks. Note If you click "Cancel" in this dialog box, no module drivers are created for this CPU, and the diagnostic screens are not updated! 6. The "Create/update diagnostic screens" dialog box opens after the completion of the generation process. Click "Yes". The function log is displayed in the "WordPad" editor. If error messages appear, rectify the errors and run the function again. Compiling and downloading an MS single station system or multiple station system ● Compile The diagnostic screens you generated or updated must be compiled and downloaded to the maintenance station. Before you compile the maintenance station, the diagnostic screens have to be created at least once or updated after configuration changes. "Area-oriented" must be set as OS compilation mode. In an MS single station system, compile the MS. In an MS multiple station system, compile the MS server. Note Clear the "Picture Tree" check box in the dialog for OS compilation if you do not want to derive the hierarchy from the plant areas. The hierarchy for the diagnostic area is created even if the check box is cleared. ● Downloading Perform the download after the compilation. If you are using an MS multiple station system, load the MS server. If you are using a redundant MS multiple station system, download the MS server and the redundant partner. You must not download an MS single station system. |
|
If I could help you, you can use the RATE button. Thank you. |
|
This contribution was helpful to
|
|
| 5/24/2016 6:50 PM | |
|
Posts: 48 Rating:
|
Hi oreca, I did the same but problem not solved . Thanks raja |
| 5/10/2022 4:30 AM | |
|
Posts: 45 Rating:
|
Hi Oreca, From your experience on this issue, during OS compilation, is it needed to check diagnostic option? or compile changes/entire is sufficient. Thanks |
Follow us on