(0)| 4/6/2009 4:41 PM | |
|
Posts: 993 Rating:
|
Hi I did not realy understood your problem. You want to create Messages with a text, date, time andtag? create a new message in the alarm control. (rigthclick > "append new line") At the properties (rightclick > "properties") confiure: Class, Type,Message Tag and Message Bit (you can set in the attachment:SetMsg1) create the message-text in the register "Text" in the field "Event" (you can set in the attachment:SetMsg2). create a alarmControl in the WinCC-picture and dobbleclick it. At the register "Message lists" add all informations you need. (you can set in the attachment:SetAlarmControl) Did that helps you or were exactly is your problem? regards cumulus AttachmentSetAlarm.zip (151 Downloads) |
| 4/6/2009 7:36 PM | |
|
Posts: 7 Rating:
|
Cumulus, Thank's for you reply! I really can not explain it right what hope, then the attachment with the picture, see if you can understand better.
Thank you. |
| 4/6/2009 9:25 PM | |
|
Joined: 3/18/2009 Last visit: 12/9/2025 Posts: 306 Rating:
|
Hello Luiz Rocha, If I understand your problem correctly, then I have bad news. See the attached snap shot of the help file. Also alinkto a discussion without any conclusion. The only round about way to acheive your requirement is to manually add the "Tag name" into a Text block of the Alarm logging. However, it is not as tedious as it sounds. Add a "User Text block"in your Alarm Logging(or you can use the existing one of Message Text) Use either excel configuration tool and edit the messages or export single messages into a comma separated text file, edit it and reimport. I hope it helps. regards. |
| 4/7/2009 7:41 PM | |
|
Posts: 7 Rating:
|
Hi Mike, |
| 4/8/2009 8:18 PM | |
|
Posts: 7 Rating:
|
Hi Mike, The PLC will S7-416-3. Greetings.
|
Follow us on